KV5x processor and external memory.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KV5x processor and external memory.

2,711件の閲覧回数
mariod
Contributor I

Hi,

i'm interested in a TWR-KV58F22M board using a KV5x processor. For my application i need to sample in parallel 4 ADCs every at 2-3Msps. I need to store the data, so i need 64MByte memory fast enough storing roughly 16MBytes/s. Is it possible? Which memory modules are suitable?

Best Mario

0 件の賞賛
返信
2 返答(返信)

2,493件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mario,

In my opinion, the KV5x is good choose.

I've attached the datasheet of the KV5x, and you can check the detail characteristics in the attachment.

However you should use the Flexbus module to interface a external RAM device, as the KV5x hasn't enough RAM size to meet your requirement.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,493件の閲覧回数
mariod
Contributor I

Thanks for your answere....i'm still confused about the Flexbus interface. Which kind of RAM modules can i connect? All other things are reall good...if memory type is clear, i will order one....

0 件の賞賛
返信