KV58F RTCS issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KV58F RTCS issue

2,143 次查看
yoramshacham
Contributor III

I've been trying to run RTCS demos on KV58F220.
I've built and download SDK 1.3 with MQX.
All the demos kept showing link but were not able to connect to the network.

Changing the adaptor from RMII to MII made it work.

Any idea with RMII is failing ?

标签 (1)
标记 (5)
0 项奖励
回复
2 回复数

2,023 次查看
miduo
NXP Employee
NXP Employee

Hi,

I am not sure which board you used, the TWR-KV58F220M or customer board? Regarding the issure, I am sorry that I have no KV58 board at hand to test. Anyway, I am pretty sure it is due to hardware and RTCS code should do some change. Please have a look at this post, hope it will be helpful.https://community.nxp.com/message/651016 

0 项奖励
回复

2,023 次查看
yoramshacham
Contributor III

Hi,

I'm using the TWR-KV58F220M board.

Complete EVM configuration - no custom additions.

0 项奖励
回复