KV58F RTCS issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KV58F RTCS issue

2,276件の閲覧回数
yoramshacham
Contributor III

I've been trying to run RTCS demos on KV58F220.
I've built and download SDK 1.3 with MQX.
All the demos kept showing link but were not able to connect to the network.

Changing the adaptor from RMII to MII made it work.

Any idea with RMII is failing ?

ラベル(1)
タグ(5)
0 件の賞賛
返信
2 返答(返信)

2,156件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

I am not sure which board you used, the TWR-KV58F220M or customer board? Regarding the issure, I am sorry that I have no KV58 board at hand to test. Anyway, I am pretty sure it is due to hardware and RTCS code should do some change. Please have a look at this post, hope it will be helpful.https://community.nxp.com/message/651016 

0 件の賞賛
返信

2,156件の閲覧回数
yoramshacham
Contributor III

Hi,

I'm using the TWR-KV58F220M board.

Complete EVM configuration - no custom additions.

0 件の賞賛
返信