KV58 CANBUS Communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KV58 CANBUS Communication

1,502件の閲覧回数
a8Chcx
Contributor IV

Hi,

I am using KV58  CANBUS to communicate the ESP32 CANBUS(Support ISO 11898-1).

1) When I try the communication between ESP32 board, it works fine.

2) When I try KV58 with K64F CANBUS, it works fine as well.

3) Then, I try KV58 CANBUS with ESP32, I cannot get it work. The difference between K64F CANBUS and ESP32 CANBUS is just MCU, all others(tranceiver, connection, and etc) are exactly same. I am wondering if it is related to timing settings?

Can anybody tell me how to fix this problem? Any suggestion?

Thanks,

Christie

 

 

0 件の賞賛
返信
1 返信

1,483件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi Christie,

Thank you so much for your interest in our products and for using our community.

I think you are correct. It is related to timing settings. If you are using the SDK examples of KV58 and K64, both bit rates are set to 1 Mb/s. Then it is only to check how the ESP32 is configured.

Hope it helps you. Please let me know if you have more questions about it.

Have a nice day!

0 件の賞賛
返信