KV58 BLDC Control with hall sensor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KV58 BLDC Control with hall sensor

7,255 次查看
a8Chcx
Contributor V

Hi,

I am using KV58 to control BLDC with hall sensors. Could you tell me if there is any demo application?

Now, I only have the senseless sample and I want to figure out commutation table for hall sensor based?

Thanks,

Christie

0 项奖励
回复
17 回复数

6,855 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Christie,

 

There is no official BLDC with hall sensors example. You can refer to the following application note which uses TWR-56F8257 and TWR-MC-LV3PH Boards.

 

BLDC Motor Control with Hall Sensors Driven by DSC

 

You can download the code from the following link.

 

https://www.nxp.com/docs/en/application-note-software/AN4413SW.zip

 

Aldo, I would recommend you to check the following community post where gives more tips about how to set this example to a TWR-KV58F board.

 

https://community.nxp.com/thread/456465

 

Hope it helps!

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

6,855 次查看
a8Chcx
Contributor V

Hi Felipe,

I can use phase A(U), B(V), C(W) to drive my DC motor. And I am using FTM1_Ch0/1 and FTM2_Ch0 to read three hall sensor status like: 4-->6-->2-->3-->1-->5. Then I converted to 0~~5 in order to use the table in sample project:

/* Commutation table */

const uint16_t bldcCommutationTableComp[16] = {

/* mask, swap */

0x0440, 0x0040, /* [0] - sector 0 */

0x0220, 0x0400, /* [1] - sector 1 */

0x0110, 0x0400, /* [2] - sector 2 */

0x0440, 0x0004, /* [3] - sector 3 */

0x0220, 0x0004, /* [4] - sector 4 */

0x0110, 0x0040, /* [5] - sector 5 */

0x0000, 0x0440, /* [6] - alignment vector (combination of sectors 0 & 1) */

0x0770, 0x0000 /* [7] - PWM off */

};

To get mask and swap. Then call the function in sample:

bool_t MCDRV_FtmSetPwmOutput(mcdrv_ftm_pwm3ph_t *this, int16_t i16Sector)

{

s_statusPass = TRUE;

this->pui32PwmBase->INVCTRL = *((this->pcBldcTable) + (2 * i16Sector + 1));

this->pui32PwmBase->OUTMASK = *((this->pcBldcTable) + (2 * i16Sector));

this->pui32PwmBase->SYNC |= (FTM_SYNC_SWSYNC_MASK);

return (s_statusPass);

}

But, my BLDC motor is not running.

Could you tell me where the possible reason is? It is related to PWMA initialization?

Do you have sample code for PWMA initialization for BLDC motor by using API?

Thanks,

Christie

0 项奖励
回复

6,855 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Christie,

 

For PWMA initialization you can refer to the InitPWMA0(); function in MC_BLDC example from de SDK.

 

Best regards,

Felipe

0 项奖励
回复

6,855 次查看
a8Chcx
Contributor V

Hi Felipe,

Do you have any BLDC initialization sample by using your SDK PWM API?

Thanks,

Christie

0 项奖励
回复

6,855 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Christie,

 

Have you checked MC_BLDC example? This example use InitPWMA0() API. This function is called by M1_MCDRV_PWM_PERIPH_INIT(); in mcdrv_twrkv58f220m.c file.

 

You can download Motor Control Examples from the following page.

https://mcuxpresso.nxp.com/en/welcome

 

Regards,

Felipe

0 项奖励
回复

6,855 次查看
a8Chcx
Contributor V

Hi Felipe,

Thank you for your information. Now, I can run my BLDC motor. But I have the following questions:

Based on commutation table in sample:

const uint16_t bldcCommutationTableComp[16] =

{

0x0440, 0x0040, // [0] - sector 0(Hall Sensor=100)---MASK A2 & B2(Phase C), Swap Phase B

0x0220, 0x0400, // [1] - sector 1(Hall Sensor=110)---MASK A1 & B1(Phase B), Swap Phase C

0x0110, 0x0400, // [2] - sector 2(Hall Sensor=010)---MASK A0 & B0(Phase A), Swap Phase C

0x0440, 0x0004, // [3] - sector 3(Hall Sensor=011)---MASK A2 & B2(Phase C), Swap Phase A

0x0220, 0x0004, // [4] - sector 4(Hall Sensor=001)---MASK A1 & B1(Phase B), Swap Phase A

0x0110, 0x0040, // [5] - sector 5(Hall Sensor=101)---MASK A0 & B0(Phase A), Swap Phase B

0x0000, 0x0440, // [6] - alignment vector (combination of sectors 0 & 1)---No MASK, Swap Phase B&C

0x0770, 0x0000 // [7] - PWM off------MASK A2&A1&A0 & B2&B1&B0(Phase A&B&C), No Swap

};

1) If I want to switch the direction, can I just change the sequence?

2) I need to switch the voltage from + to '-' in order to switch the direction because I saw this in your BLDC controller application?

If I just switch the sequence of commutation table, it won't work? I have to switch voltage?

ex: 0x0440, 0x0040, // [0] - sector 0(Hall Sensor=100)---MASK A2 & B2(Phase C), Swap Phase B---For CW

      0x0440, 0x0004, // [0] - sector 0(Hall Sensor=100)---MASK A2 & B2(Phase C), Swap Phase A---For CCW

What is the better way to do the direction switching?

Thanks,

Christie

0 项奖励
回复

6,855 次查看
a8Chcx
Contributor V

Hi Felipe,

I have the following problem during my BLDC testing:

I tried to do commutation first, then set duty of PWM, I am always going the opposite direction first for short time, then go back to the right direction. Is there any way to avoid this? Any idea, why?

Thanks,

Christie 

0 项奖励
回复

6,855 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Christie,

 

I am sorry for my late reply.

 

Could you please verify if the hall sensors are reading correctly during the time the motor goes to the opposite direction?

 

Also, please double check the position of the sensors as they must be placed at 120 degrees apart around the rotor.

 

Best regards,

Felipe

0 项奖励
回复

6,855 次查看
a8Chcx
Contributor V

Hi Felipe,

I apply the 90% PWM for CW direction and 100%-90% = 10% PWM for CCW to three phase based on the same commutation sample and works fine for now.

One more question: When I move the motor in CW and CCW with the same PWM duty, I can see CCW direction is much slower than CW direction...

Could you tell me if you experience the same issue and how to fix it?

Thanks,

Christie

0 项奖励
回复

6,855 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Christie,

 

You shouldn’t have this behavior when changing to CWW direction.

 

Could you please explain how are you setting the table for CCW direction? Are you reversing the polarity of the phases? Please take a look to the following video to see an explanation on how to make commutation table for CW and CCW direction.

https://www.nxp.com/video/bldc-commutation-programming:V7-BLDC-COMMUTATION-IMPLEMENTATION?lang=en&la...

 

I hope it helps!

 

Best regards,

Felipe

0 项奖励
回复

6,855 次查看
a8Chcx
Contributor V

Hi Felipe,

I am using the same commutation table and change the PWM duty for V+ or V-.

Ex. For CW, I am using 90% of PWM duty to apply to 3 phases and SWAP or MASK based on table.

For CCW, I am using 10% of PWM duty to apply to 3 phases and SWAP or MASK based on table.

It works fine for both directions. Only problem is now that CCW speed is much slower than CW when I applied 90% of PWM. It is getting closer when I applied 50% of PWM.

I am not sure what the reason is? Maybe, it is related to hall sensor alignment?

Thanks,

Christie

0 项奖励
回复

6,855 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Christie,

 

That may be one reason.  Please double check the position of the sensors as they must be placed at 120 degrees apart around the rotor.

 

Regards,

Felipe

0 项奖励
回复

6,855 次查看
a8Chcx
Contributor V

Hi Felipe,

I got lots of noise from hall sensor to cause the commutation issue.

Is there any way to filter the noise on hall sensor from MCU or signal?

Thanks,

Christie

0 项奖励
回复

6,855 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Christie,

 

You could try with a bypass capacitor or a RC Low Pass Filter and see how it works. I recommend you to check your sensor's specifications.

 

Best regards,

Felipe

0 项奖励
回复

6,855 次查看
a8Chcx
Contributor V

Hi Felipe,

After adding some filtering on hall sensors, it works fine. Thanks.

I had the following issue now:

1) I am trying to use the ramp control to add the power slowly and causes the motor start-up problem. Sometime, I can't start motor even with full power applied on it. When it is the low power, motor keeps bouncing back and force...

2) If I applied full power, no ramp control, it works fine...

Do you experience the similar issue and how to fix it?

Thanks,

Christie

0 项奖励
回复

6,855 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Christie,

 

As this question is different from the original question of this post. Could you help me creating another community thread for this question?

 

Best regards,

Felipe

0 项奖励
回复

6,855 次查看
a8Chcx
Contributor V

No problem.

0 项奖励
回复