KV4 ADC calibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,373件の閲覧回数
zorrotz
Contributor III

Hello,

Some Kinetis microcontrollers, like KV31, include a ADC self-calibration function.

Reading KV4 documentation i don't see any reference to this function, so doesn't KV4 include ADC self-calibration?

Thanks

 

0 件の賞賛
返信
1 解決策
2,365件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi zorrotz,

 No, KV4x 12-bit cyclic ADC hasn't calibration function, it is different with the ADC on other KV series devices.

 

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,366件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi zorrotz,

 No, KV4x 12-bit cyclic ADC hasn't calibration function, it is different with the ADC on other KV series devices.

 

Regards,

Jing

0 件の賞賛
返信
2,362件の閲覧回数
zorrotz
Contributor III

Thank you!

Regards

zorrotz

0 件の賞賛
返信