KSDSK v1.3 flash driver while clock change

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDSK v1.3 flash driver while clock change

ソリューションへジャンプ
2,180件の閲覧回数
renka
Contributor II

Hi,

I'am currently working with K26f processor with KDS3.2 and KSDSK v1.3. Core clock is 180Mhz,Flash Clock is 25.71 Mhz as Processor Expert recommends...  I know that it's a high speed clock mode and any flash activities are prohibited in this mode. In oder to solve it ,i have use by CLOCK_SYS_SetConfiguration()  with core clock 120Mhz,Flash clock is 24Mhz, before starting my flash driver (like Flash erase,flash program) activities.But  any way,i receive Flash ERROR_ACCEER error. It seems like flash driver didn't know about core/flash clock changing....

Please help me.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,113件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Make sure that the processor in in RUN mode and not HSRUN mode. In HSRUN mode it will not work, even if the clocks are slow.

Study also the requirement for changing modes and clocks since there are some rules to be observed.

Regards

Mark

元の投稿で解決策を見る

2 返答(返信)
2,114件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Make sure that the processor in in RUN mode and not HSRUN mode. In HSRUN mode it will not work, even if the clocks are slow.

Study also the requirement for changing modes and clocks since there are some rules to be observed.

Regards

Mark

2,113件の閲覧回数
renka
Contributor II

Thank you.

0 件の賞賛
返信