KM3x - Filter-based algorithm source code for metering Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KM3x - Filter-based algorithm source code for metering Application

2,811 Views
Deejay
Contributor III

Hi,

There is a reference design (DRM143) based on KM3x for a single phase metering application using filter-based algorithm (as covered in AN4265).

DRM143

http://cache.freescale.com/files/32bit/doc/ref_manual/DRM143.pdf?fasp=1&WT_TYPE=Application%20Notes&...

AN4265

http://cache.freescale.com/files/32bit/doc/app_note/AN4265.pdf?fasp=1&WT_TYPE=Application%20Notes&WT...

The source code is built with libraries (fraclib.a, meterlib.a).

Where can I get the source code for those libraries?

Thanks.

Regards,

Devan

0 Kudos
Reply
2 Replies

1,995 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Devan,

The fraclib.a and meterlib library source code need to sign a NDA agreement.

After you sign the NDA agreement, you could contact with your local Freescale Distributor to get the source code.

The distributor network could be found from here.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,995 Views
Deejay
Contributor III

Hi Ma Hui,

Thanks for the response.

In fact, I'm an FAE working for a distributor and this is for one of our customers. I will organize an NDA with the customer.

Best regards,

Devan

0 Kudos
Reply