KM35 PORT STRUCTURE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KM35 PORT STRUCTURE

ソリューションへジャンプ
3,987件の閲覧回数
jun1
Contributor V

 

Hi.

The KE04 Sub-Family Reference Manual describes the structure of the port, but the Kinetis KM35 Sub-Family Reference Manual does not seem to.
1. Is there any material for the port structure of KM35?
2. When using the KM35 port with UART, does the open drain setting also work?

 

thanks.

 

ラベル(1)
0 件の賞賛
返信
1 解決策
3,967件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi jun,

1. You can refer to this picture. This is KE16Z pin structure. But I think KM35 is similar to it.

jingpan_0-1624437655937.png

 

2. The functions apply across all digital pin muxing modes and individual peripherals do not override the configuration in the Pin Control register. For example, if an I2C function is enabled on a pin, that does not override the pullup or open drain configuration for that pin.

 

Regards,

Jing

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,968件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi jun,

1. You can refer to this picture. This is KE16Z pin structure. But I think KM35 is similar to it.

jingpan_0-1624437655937.png

 

2. The functions apply across all digital pin muxing modes and individual peripherals do not override the configuration in the Pin Control register. For example, if an I2C function is enabled on a pin, that does not override the pullup or open drain configuration for that pin.

 

Regards,

Jing

 

0 件の賞賛
返信