KM35 PORT STRUCTURE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KM35 PORT STRUCTURE

Jump to solution
4,046 Views
jun1
Contributor V

 

Hi.

The KE04 Sub-Family Reference Manual describes the structure of the port, but the Kinetis KM35 Sub-Family Reference Manual does not seem to.
1. Is there any material for the port structure of KM35?
2. When using the KM35 port with UART, does the open drain setting also work?

 

thanks.

 

Labels (1)
0 Kudos
Reply
1 Solution
4,026 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi jun,

1. You can refer to this picture. This is KE16Z pin structure. But I think KM35 is similar to it.

jingpan_0-1624437655937.png

 

2. The functions apply across all digital pin muxing modes and individual peripherals do not override the configuration in the Pin Control register. For example, if an I2C function is enabled on a pin, that does not override the pullup or open drain configuration for that pin.

 

Regards,

Jing

 

View solution in original post

0 Kudos
Reply
1 Reply
4,027 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi jun,

1. You can refer to this picture. This is KE16Z pin structure. But I think KM35 is similar to it.

jingpan_0-1624437655937.png

 

2. The functions apply across all digital pin muxing modes and individual peripherals do not override the configuration in the Pin Control register. For example, if an I2C function is enabled on a pin, that does not override the pullup or open drain configuration for that pin.

 

Regards,

Jing

 

0 Kudos
Reply