KM34 is always in reset after power ON.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KM34 is always in reset after power ON.

1,236 次查看
armaram
Contributor III

Our KM34 device has the reset pin always low. The device seems to be keeping it low.

Due to this I am unable to program the device.

Any help or guidance is greatly appreciated.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,054 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Arvind Reddy Maram,

   Is this KM34 board designed by yourself? Have you downloaded the code to this chip before?

  To an empty KM34 chip, the reset pin have the sawtooth wave is correct, after the chip is flashed, the reset pin will be high.

  I think, you can use the JLINK associated with the JLINK command to check whether you can connect the ARM core or not?

  If you can't find the core, it means your board hardware have problems. RESET is low won't influence the flash download.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复