KM33Z128 boots in VLPR mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KM33Z128 boots in VLPR mode

992件の閲覧回数
miguelportela
Contributor I

Hello,

    I am working in a project that uses the microcontroller KM33Z128AM. I realized that some chips are booting randomly in VLPR mode. After that, when configuring the clock, the devices performs a reset. The device then enters in a infinite loop of resets. The bit EXE_MODE in FTFL_OPT register is zero. Therefore, I think the microcontroller should be always exit from reset in RUN mode. In which other situation could the device boot in VLPR mode?

Thank you.

BR

タグ(1)
0 件の賞賛
返信
0 返答(返信)