KL8x current draw for LP Trusted Crypto (LTC)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL8x current draw for LP Trusted Crypto (LTC)

1,433件の閲覧回数
andreiscurtu
Contributor I

Hello,

I'm looking into low power uCs for a battery operated application. I don't seem to find the info on the power draw for the LTC (crypto) module available in the KL8x. I assume this may be a large value due to the complexity of the encryption/decryption operation so I should definitely consider it for the overall power consumption.

I'm looking in the KL82P121M72SF0 document and this info doesn't appear to be listed.

     Should I be looking elsewhere?

Regards,

Andrei

ラベル(2)
0 件の賞賛
返信
1 返信

1,227件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Please accept my apologies for the late response

Hope that the below information is helpful for you.

KL81Z128 @96MHz

SHA256                                 --- Max 17.88mA

AES(128,192,256)                 --- Max 20.10mA

3DES                                     --- Max 19.30mA

RSA2048                               --- Max 24.10mA

ECDSA(192,384,256,512)     --- Max 24.50mA

Regards

Vicente Gomez

0 件の賞賛
返信