KL82 Cryptography Performance?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL82 Cryptography Performance?

5,123件の閲覧回数
q1220200
Contributor III

The KL82 series have a "low power" trusted cryptography (LTC) module, however, the datasheet explicitly states that there are "no [electrical] specifications necessary for the device's security and integrity modules."

How can we know that this module is truly "low power", and what does that even mean?

What kind of computational performance does this module offer when processing the various cryptographic functions?

I'm presently doing research into elliptic curve cryptography for IoT, so the specifics of the unit's performance are relevant to my work.

Does anyone know where I can find some solid, published data on this?

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

5,059件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @q1220200 

The LTC module is part of our Cryptographic IP’s and acquires the low power naming because it provides better performance, reduces power consumption and code   than other of our IPs in certain applications. Please refer to the wolfssl article about the K8x / KL8 LTC NXP Kinetis K8X LTC support for PKI (RSA/ECC) with #TLS13

Generally, electrical characteristics are not provided in the datasheets. For example, the current consumption of the Module itself, it is difficult to characterize because one cannot separate  with ease the CPU and LTC module current consumption. From this post  KL8x current draw for LP Trusted Crypto (LTC) you can get an idea of a test being made on a KL81Z128 @96MHz

 Regarding, performance, you can check our FRDM-KL82z SDK example wolfssl_benchmark. In the case you were not able to run the demo you will find my results my results.

Br,

Diego. 

 

 

 

 

0 件の賞賛
返信

5,099件の閲覧回数
q1220200
Contributor III

...

0 件の賞賛
返信

5,105件の閲覧回数
mjbcswitzerland
Specialist V

Hi

I have some KL82 LTC performance comparisons (with SW and other crypto modules) at https://www.utasker.com/docs/uTasker/uTasker_Cryptography.pdf

But these are only for AES and SHA and I don't think the module can help with elliptic curves.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or product development requirements

 

0 件の賞賛
返信

5,097件の閲覧回数
q1220200
Contributor III

Thanks for the link Mark.

The KL82's LTC definitely does elliptic curves, there's pages on it in the sub family manual, just no mention of performance characteristics etc..

0 件の賞賛
返信

5,088件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Thanks for the heads up - I haven't used Elliptic curves and since the MMCAU doesn't have support for public key acceleration I was assuming that the LTC would be the same, which was wrong...

Thanks again

Regards

Mark

 

 

0 件の賞賛
返信