KL82 Cryptography Performance?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL82 Cryptography Performance?

5,141 Views
q1220200
Contributor III

The KL82 series have a "low power" trusted cryptography (LTC) module, however, the datasheet explicitly states that there are "no [electrical] specifications necessary for the device's security and integrity modules."

How can we know that this module is truly "low power", and what does that even mean?

What kind of computational performance does this module offer when processing the various cryptographic functions?

I'm presently doing research into elliptic curve cryptography for IoT, so the specifics of the unit's performance are relevant to my work.

Does anyone know where I can find some solid, published data on this?

Thanks in advance.

Labels (1)
0 Kudos
Reply
5 Replies

5,077 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @q1220200 

The LTC module is part of our Cryptographic IP’s and acquires the low power naming because it provides better performance, reduces power consumption and code   than other of our IPs in certain applications. Please refer to the wolfssl article about the K8x / KL8 LTC NXP Kinetis K8X LTC support for PKI (RSA/ECC) with #TLS13

Generally, electrical characteristics are not provided in the datasheets. For example, the current consumption of the Module itself, it is difficult to characterize because one cannot separate  with ease the CPU and LTC module current consumption. From this post  KL8x current draw for LP Trusted Crypto (LTC) you can get an idea of a test being made on a KL81Z128 @96MHz

 Regarding, performance, you can check our FRDM-KL82z SDK example wolfssl_benchmark. In the case you were not able to run the demo you will find my results my results.

Br,

Diego. 

 

 

 

 

0 Kudos
Reply

5,117 Views
q1220200
Contributor III

...

0 Kudos
Reply

5,123 Views
mjbcswitzerland
Specialist V

Hi

I have some KL82 LTC performance comparisons (with SW and other crypto modules) at https://www.utasker.com/docs/uTasker/uTasker_Cryptography.pdf

But these are only for AES and SHA and I don't think the module can help with elliptic curves.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or product development requirements

 

0 Kudos
Reply

5,115 Views
q1220200
Contributor III

Thanks for the link Mark.

The KL82's LTC definitely does elliptic curves, there's pages on it in the sub family manual, just no mention of performance characteristics etc..

0 Kudos
Reply

5,106 Views
mjbcswitzerland
Specialist V

Hi

Thanks for the heads up - I haven't used Elliptic curves and since the MMCAU doesn't have support for public key acceleration I was assuming that the LTC would be the same, which was wrong...

Thanks again

Regards

Mark

 

 

0 Kudos
Reply