[KL46Z] Magnetometer MAG3110 interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[KL46Z] Magnetometer MAG3110 interrupt

1,615 Views
rafcio100
Contributor I

I have a problem with configuring MAG3110  interrupts. The PTD1 pin is always HIGH.

#include "mbed.h"
#include "MAG3110.h"
MAG3110 mag(PTE25, PTE24);
Serial pc(USBTX, USBRX);
MotionSensorDataCounts mag_raw;
InterruptIn mag_interrupt(PTD1);

void flip() {
    mag.getAxis(mag_raw);
    float x;
    x = ((float) mag_raw.x) / 10.0f;
    pc.printf("Mag x=%4.1f\r\n", x);
    wait(1.0);
}

int main(void){
    pc.baud(9600);
    mag.enable();
    mag_interrupt.rise(&flip);
    while(1) {
      sleep();
    }
}
0 Kudos
Reply
2 Replies

1,514 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Rafal Jablonski,

   About the MAG3110 interrupt usage, you need to follow these step:

pastedImage_1.png

   Please check it on your side, do you finish these step?

If you still have question after the test, please tell me the updated information.

 

Wish it helps you!

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,514 Views
rafcio100
Contributor I

Hi Kerry Zhou,

I was finished this steps before I wrote that post, but it doesn't work. Pin INT is always HIGH, even when I read 0x01 OUT_X_MSB register.

0 Kudos
Reply