Hi @rppolicy ,
You are uing the TPM module right? Could give more details of the clock being used as source for the timer? Please notice that the clock accuracy is different for the internal reference clocks:
• 48MHz high accuracy (up to 0.5%) internal reference clock
• 8MHz/2MHz high accuracy (up to 3%) internal reference clock
Could you also provide more details of the frequency of the input signal you are capturing? Note that the maximum frequency for the channel input signal to be detected correctly is counter clock divided by 4.
Regarding the AN5142, you are correct, this FlexTimer module is not present in the KL46Z devices.
Regards,
Carlos Mendoza
Field Applications Engineer