KL46Z CAN Bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL46Z CAN Bus

1,310件の閲覧回数
andrehart
Contributor I

Hey together,

anyone, who worked with the KL46Z Board and tried a CAN communication?
Which componends you used? MCP2515?
Maybe you got some informations for me :smileyhappy:

Thank you

Andre

0 件の賞賛
返信
1 返信

1,235件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Andre Hartmann,

    KL46 chip don't have the CAN module, so you can't use the KL46 directly with CAN bus.

    If you want to use it, you need to use the external CAN module. You can use MCP2515 which you mentioned, I find it is the SPI interface, which can communicate with the MCU(KL46).

   But we don't have the sample code for it, you need to finish it by yourself.

   About the SPI driver, you can refer to our KSDK for FRDM-KL46, there have the SPI driver.

  Welcome to MCUXpresso | MCUXpresso Config Tools 

SDK builder, then choose FRDM-KL46, generate the code and download it.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信