KL46 SPI0 FIFO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL46 SPI0 FIFO

1,364件の閲覧回数
eric_b
Contributor I

I've been working with a FRDM KL46Z and using SPI1 with the FIFO enabled. For my final application I will need to use SPI0 and I thought this would be an easy change with PE in KDS 3.2.0. However, PE does not let me select a HW buffer of 8 (FIFO enabled)  for SPI0. It says, "ERROR: The device doesn't support this setting!" I've reviewed the Reference Manual and I have not found anything indicating that this feature is not available for SPI0. Is there something I'm overlooking or is this a bug in PE?

ラベル(1)
0 件の賞賛
返信
1 返信

1,306件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Eric,

I am sorry to tell you that the SPI0 of KL46 does not 'include a 4-deep FIFO'.

SPI1 includes a 4-deep FIFO.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信