KL28Z512VLL7 Issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,096件の閲覧回数
kaimengtan
Contributor I

Hi,

I have 2 KL28Z for my startup projects, both are KL28Z512VLL7. I'm still very new to this board.

However, I'm facing a few weird issues as below:

Board 1:

My computer can't detect any disk drive after plugged in, the only disk drive that I'm able to detect is the bootloader.

Board 2:

Fortunately the disk drive able to get detected and from device manager it shows up as COM16.

But, I can't connect to the board even using the putty or teraterm terminal. I have set the baud rate to 115200 but still no luck.

Then, I installed KDS 3.2, SDK2.0 KL28Z downloaded from FRDM-KL28Z|Freedom Development Platform|Kinetis MCU|NXP & also JLink V6 etc. I imported hello_world demo project, compile and debug using Jlink. It can't even run and the program already dead when running startup.S file.

Is there anything that I can do? Maybe restore the boards or something else?

Looking forward for reply. I need to proceed & rushing for the deadline. Thanks in advance.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
3,881件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello Kai,

somehow your Windows 7 machine does things like a Windows 10 machine. Are you sure you never have connected the board to a Windows 10 machine?

Board 1 reacts as if there is no debug application loaded (see https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/).

About serial connection: this is a UART-to-USB connection. So your KL28 has to communicate something to the UART. This is in the application domain, so your application on the KL28 has to do something on the UART.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,881件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello Kai,

what host operating system are you using? For board 1, what is the small green OpenSDA LED doing?

If you are using Windows 10, then this article (https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/ ) might be helpful.

For the board 2: I believe the default application (factory installed) on the board does not communicate through the OpenSDA serial port, so you won't see any traffic there.

I hope this help,

Erich

0 件の賞賛
返信
3,881件の閲覧回数
kaimengtan
Contributor I

Hi Erich,

I'm using Windows 7.

For board 1, the small green openSDA LED doesn't even light up, it only started to blink when I put it into bootloader mode.

For board 2, the openSDA LED doesn light up. Quoted this " I believe the default application (factory installed) on the board does not communicate through the OpenSDA serial port, so you won't see any traffic there." if default application does not communicate through openSDA, anything I can do to resolve it? Flashing some bootloader etc?

PS: Below are snapshot of my disk drive in normal mode & bootloader mode. The files inside looks strange.

Capture.JPG

Capture1.JPG

PS2: I downloaded J-Link OpenSDA - Board-Specific Firmwares from segger.com for KL28Z.

Now both of my boards can enumerate disk drive in normal mode. But it doesn't solve the program issue when running Jlink debugging in KDS.

Thanks

0 件の賞賛
返信
3,882件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello Kai,

somehow your Windows 7 machine does things like a Windows 10 machine. Are you sure you never have connected the board to a Windows 10 machine?

Board 1 reacts as if there is no debug application loaded (see https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/).

About serial connection: this is a UART-to-USB connection. So your KL28 has to communicate something to the UART. This is in the application domain, so your application on the KL28 has to do something on the UART.

I hope this helps,

Erich

0 件の賞賛
返信
3,881件の閲覧回数
kaimengtan
Contributor I

Hi Erich,

I can't confirm on whether they have connected to windows 10 OS before as I only received the boards from others few days ago, and the previous guys might have already did something on it thus causing it doesn't work as what I'm expected. And yes, I found your youtube video while I'm searching for possible recovery solutions. It works back after I downloaded FW from segger.com

Another issue is, I'm trying to run hello_world demo project on KL28Z but it doesn't work.

I have imported the project, build and debug with hello_world_frdmkl28z debug jlink. Somehow it just ended while running startup_MKL28Z7.s, the console will only reach until "Starting target CPU". Can you provide some advice on what is happening here?

I connected the board to my PC via mini-B at the openSDA port.

Thank you very much.

Log:

SEGGER J-Link GDB Server V6.00b Command Line Version

JLinkARM.dll V6.00b (DLL compiled Jul 27 2016 18:18:11)

-----GDB Server start settings-----

GDBInit file:                  none

GDB Server Listening port:     2331

SWO raw output listening port: 2332

Terminal I/O port:             2333

Accept remote connection:      localhost only

Generate logfile:              off

Verify download:               on

Init regs on start:            on

Silent mode:                   off

Single run mode:               on

Target connection timeout:     0 ms

------J-Link related settings------

J-Link Host interface:         USB

J-Link script:                 none

J-Link settings file:          none

------Target related settings------

Target device:                 MKL28Z512xxx7

Target interface:              SWD

Target interface speed:        auto

Target endian:                 little

Connecting to J-Link...

J-Link is connected.

Firmware: J-Link OpenSDA 2 compiled Aug  1 2016 15:06:07

Hardware: V1.00

S/N: 621000000

Checking target voltage...

Target voltage: 3.30 V

Listening on TCP/IP port 2331

Connecting to target...Connected to target

Waiting for GDB connection...Connected to 127.0.0.1

Reading all registers

Read 4 bytes @ address 0x00000000 (Data = 0xFFFFFFFF)

Target interface speed set to 30 kHz

Resetting target

Halting target CPU...

...Target halted (PC = 0x1C000140)

R0 = 1C000460, R1 = 1FFFAC90, R2 = 1FFFA000, R3 = 00080000

R4 = 1FFFAD20, R5 = 1C000460, R6 = 1FFFA000, R7 = 00000000

R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000

R12= 00000000, R13= 1FFFB5C8, MSP= 1FFFB5C8, PSP= EFFFF7FC

R14(LR) = 1C001761, R15(PC) = 1C000140

XPSR 21000000, APSR 20000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Select auto target interface speed (1429 kHz)

Flash breakpoints enabled

Semi-hosting enabled (Handle on BKPT)

Wrong client mask. Semihosting I/O not changed.

Downloading 320 bytes @ address 0x00000000 - Verified OK

Downloading 16 bytes @ address 0x00000400 - Verified OK

Downloading 8556 bytes @ address 0x00000410 - Verified OK

Downloading 8 bytes @ address 0x0000257C - Verified OK

Downloading 4 bytes @ address 0x00002584 - Verified OK

Downloading 4 bytes @ address 0x00002588 - Verified OK

Downloading 104 bytes @ address 0x0000258C - Verified OK

Writing register (PC = 0x48060000)

Read 4 bytes @ address 0x00000648 (Data = 0x480CB672)

Resetting target

Halting target CPU...

...Target halted (PC = 0x1C000140)

Read 2 bytes @ address 0x00001C0A (Data = 0xF7FE)

Read 2 bytes @ address 0x00001C0A (Data = 0xF7FE)

Read 2 bytes @ address 0x00001C0A (Data = 0xF7FE)

R0 = 00000000, R1 = B480A602, R2 = 00000350, R3 = 0C4E6B61

R4 = 1FFFA68C, R5 = 1FFFA6AC, R6 = 1FFFA6AC, R7 = 00000000

R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000

R12= 1FFFA600, R13= 1FFFB5C8, MSP= 1FFFB5C8, PSP= EFFFF7FC

R14(LR) = 1FFFA32F, R15(PC) = 1C000140

XPSR 61000000, APSR 60000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Reading all registers

Read 4 bytes @ address 0x1C000140 (Data = 0x480EB672)

Setting breakpoint @ address 0x00001C0A, Size = 2, BPHandle = 0x0001

Starting target CPU...

0 件の賞賛
返信
3,881件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Kai,

unfortunately I do not have that board. But I would recommend that you stop the target with the debugger to see where it is executing code? Maybe it did not reach somehow main() because of an exception?

Erich

0 件の賞賛
返信
3,881件の閲覧回数
kaimengtan
Contributor I

Hi Erich,

Somehow I managed to get it work by changing the memory map in the linker file.

I shrink the front end & back end of the SDRAM memory block and then it works flawlessly now. Strange but at least now I can proceed further. :smileyhappy:

I will look back this issue when I have some time later on.

Thanks again for everything.

0 件の賞賛
返信