KL27Z128 USB HID Mouse remote wakeup issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KL27Z128 USB HID Mouse remote wakeup issue

跳至解决方案
3,050 次查看
waynelin
Contributor I

Dear

KL27 support remote wake but I use KL27Z128 I can’t find remote wake in KL43 sample code is this function ready in KL43 and support KL27Z128.

Best regards,

Wayne

1 解答
2,670 次查看
cutworth
NXP Employee
NXP Employee

Hi Wayne,

I have finished testing the HID mouse remote wakeup demo on FRDM-KL43 board. Attached the demo project in IAR. 

Before you run the demo, please make sure you have enabled USB wakeup support in PC BIOS. Also you need to plug in AC power with your laptop, otherwise you will not be able to wakeup laptop with HID mouse. See below image for example.

pastedImage_1.png

When you run the demo, you will see console output as follows first and HID mouse detected on PC and it circles in one square.

USB device HID mouse demo

When you close your laptop lid, you will see PC suspended and console output as follows.
USB device remote wakeup state: 1
USB device start suspend
USB device suspended.
Please Press 'SW3' to remote wakeup the host.

When you press SW3 on FRDM-KL43 board, you will see console output as follows and PC waking up by HID mouse.
Remote wakeup the host.
USB device start resume
USB device resumed.
USB device remote wakeup state: 0

Finally please note you need to power OPENSDA USB port to another PC which does not suspend at all, otherwise the board will be removed power when the laptop suspends

Hao

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,670 次查看
cutworth
NXP Employee
NXP Employee

Hi Wayne,

I have one demo which works on K65 tower board for showing suspend/resume feature. I am working on porting this to FRDM KL43 board. Will post it here once I finished testing the demo. 

Hao

2,671 次查看
cutworth
NXP Employee
NXP Employee

Hi Wayne,

I have finished testing the HID mouse remote wakeup demo on FRDM-KL43 board. Attached the demo project in IAR. 

Before you run the demo, please make sure you have enabled USB wakeup support in PC BIOS. Also you need to plug in AC power with your laptop, otherwise you will not be able to wakeup laptop with HID mouse. See below image for example.

pastedImage_1.png

When you run the demo, you will see console output as follows first and HID mouse detected on PC and it circles in one square.

USB device HID mouse demo

When you close your laptop lid, you will see PC suspended and console output as follows.
USB device remote wakeup state: 1
USB device start suspend
USB device suspended.
Please Press 'SW3' to remote wakeup the host.

When you press SW3 on FRDM-KL43 board, you will see console output as follows and PC waking up by HID mouse.
Remote wakeup the host.
USB device start resume
USB device resumed.
USB device remote wakeup state: 0

Finally please note you need to power OPENSDA USB port to another PC which does not suspend at all, otherwise the board will be removed power when the laptop suspends

Hao

0 项奖励
回复
2,670 次查看
bobpaddock
Senior Contributor IV

In one of the other treads a while ago:

"Kan_Li Employee:

The AE team has reported this issue to the doc team, this
version will be updated soon, bit 2-3 of USBx_CTL are
available just as other parts with OTG, and bit3 has some
description issue, which will be updated as well. bit3 of
USBx_CTL isn't used for Host only, and KL27 can support remote
wakeup feature."

from notes in my USB code.

0 项奖励
回复