KL27Z FLASH_Erase() causing reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL27Z FLASH_Erase() causing reset

ソリューションへジャンプ
2,545件の閲覧回数
robertpoor
Senior Contributor I

Short form:

When I run my code, I'm getting system resets somewhere inside:

flash_command_sequence.6917() at fsl_flash.c:2,554 0x4388 
FLASH_Erase() at fsl_flash.c:731 0x4880 

Details:

I'm running code which is closely modeled after the Flash programming example in:

boards/frdmkl27z/driver_examples/flash/pflash/pflash.c

However, when I call FLASH_Erase(), the system resets.  (And since my call to FLASH_Erase() is in the initialization code, it resets repeatedly.)  Unfortunately, when I single step into FLASH_Erase(), the call to FLASH_Erase() completes normally which makes it difficult to pinpoint the problem.  [UPDATE: at least I thought it did.  Now it seems to reset repeatedly when I try to step into callFlashRunCommand(), aka flash_command_sequence.] 

The system is powered off USB and a SEGGER JLink, so I think it has sufficient power.

I notice the call flash_command_sequence() has comments about executing position-independent code in memory -- is it possible that the code isn't properly loaded into memory?

Any idea what might be causing this, and what I can do to work around it?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,279件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Make sure that you run the code from SRAM and with interrupts disabled.

Regards

Mark

Professional support for Kinetis: http://www.utasker.com/index.html
Remote desktop one-on-one coaching: http://www.utasker.com/services.html
Getting started to expert videos: https://www.youtube.com/results?search_query=utasker+shorts

元の投稿で解決策を見る

2 返答(返信)
2,280件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Make sure that you run the code from SRAM and with interrupts disabled.

Regards

Mark

Professional support for Kinetis: http://www.utasker.com/index.html
Remote desktop one-on-one coaching: http://www.utasker.com/services.html
Getting started to expert videos: https://www.youtube.com/results?search_query=utasker+shorts

2,279件の閲覧回数
robertpoor
Senior Contributor I

I independently discovered that interrupts were indeed the problem: I had implemented a regular timer interrupt.  Turning that off during the time I was writing to flash fixed the problem.

Thanks!

0 件の賞賛
返信