KL27 Microcontroller, supply current.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KL27 Microcontroller, supply current.

跳至解决方案
2,722 次查看
sebastianbaez
Contributor I

I'm using the KL27 Microcontroller in an Energy Harvesting application, do I need 120mA supply current, even if I'm going to use it in low power modes?

Best Regards.

SBB.

标记 (2)
1 解答
2,521 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sebastian Baez,

    120mA is the max data for the MCU supply current.

    If your MCU power consumption is not very large, you don't need to use 120mA, you can use smaller power supply current.  This data is just the max data definition.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,521 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sebastian baez,

    About the KL27 power consumption, you can refer to our KL27 datasheet, you will find all the power mode consumption, include RUN, low power consumption.

   http://www.nxp.com/assets/documents/data/en/data-sheets/KL27P64M48SF6.pdf 

Page 10.

  You can find, even in the RUN mode,Run mode current¡ª48M HIRC mode, running CoreMark in Flash all peripheral clock disable 48 MHz core/24 MHz flash, VDD = 3.0 V, the consumption is below 10mA.

Wish it helps you!
Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,521 次查看
sebastianbaez
Contributor I

I appreciate your answer,

yes I already seen that power comsumption table. What I mean, is that in page 6 of the datasheet (Voltage and current operating ratings), says that the MCU needs a supply current of 120 mA.

I'm kind of confused,
Hope you help me.

0 项奖励
回复
2,522 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sebastian Baez,

    120mA is the max data for the MCU supply current.

    If your MCU power consumption is not very large, you don't need to use 120mA, you can use smaller power supply current.  This data is just the max data definition.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复