KL26 USB microphone

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL26 USB microphone

1,448 Views
martindusek
Contributor V

We have a device that is based on KL26 MCU and we came across an idea to implement USB microphone using that device. Is it practical to implement USB microphone using KL26? The device already runs Freescale USB stack (HID device) and for microphone it would have to run also USB audio class. Sampling frequency should be 22 kHz.

0 Kudos
Reply
1 Reply

1,314 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Martin,

First of all, you can go for down the Kinetis SDK through the link as below.

And in the Kinetis SDK, it has contained various kind of USB demo which definitely includes the USB audio class.

Software Development Kit for Kinetis MCUs|Freescale
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply