KL26 UART mark and space parity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL26 UART mark and space parity

Jump to solution
1,264 Views
chuanchuanli
Contributor I

I want to use serial port. I have some questin about the UART0/UART1 of KL26 . 

1.Can I use UART0 mark parity on 7-bit data characters?

2. can I receiver and transmitter use 7 bit data characters through UART0/UART1.

3.some question on picture.6.png

1 Solution
1,088 Views
Rick_Li
NXP Employee
NXP Employee

Hi Chuanchuan Li,

As said by the reference, only 10-bit, 9-bit and 8-bit (10-bit is only supported in UART0) are supported in KL26.

you can not use 7-bit data character.

regarding the question on the attached image, the bit M in UART0 and UART1/2 has the same function. the description for bit M in both chapter mean same thing.

hope it help!

View solution in original post

1 Reply
1,089 Views
Rick_Li
NXP Employee
NXP Employee

Hi Chuanchuan Li,

As said by the reference, only 10-bit, 9-bit and 8-bit (10-bit is only supported in UART0) are supported in KL26.

you can not use 7-bit data character.

regarding the question on the attached image, the bit M in UART0 and UART1/2 has the same function. the description for bit M in both chapter mean same thing.

hope it help!