KL25Z32VFM4 controller selection with Code warrior 10.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KL25Z32VFM4 controller selection with Code warrior 10.3

跳至解决方案
1,947 次查看
Embionics
Contributor III

Hello Sir,

I want to work with MKL25Z32VFM4(60 pin) controller with Code warrior 10.3.

But when i am trying to create a new BareBoard project with this controller ,options are as

MKL25Z32

MKL25Z64

MKL25Z128

After selecting MKL25Z32 by default MKL25Z32VLK4(80 pin) this controller is getting selected.

Is it possible to select particular MKL25Z32VFM4(60 pin) controller?

i want to select this as there are some pins are not present in MKL25Z32VFM4(60 pin) as compare to MKL25Z32VLK4(80 pin).

I want to generate code for on ADC with MKL25Z32VFM4(60 pin).

There is no VrefH and VrefL pin in MKL25Z32VFM4(60 pin) controller.

But as MKL25Z32VLK4(80 pin) is getting selected i can see the option of reference voltage selection.

How it will select reference voltage forMKL25Z32VFM4(60 pin) controller ?

Regards,

Amreen

标签 (1)
0 项奖励
回复
1 解答
1,738 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

MCU10.3 is rather old, the most current release is 10.5.

I checked things in MCU 10.5, and I have the VFM4 package available.

You might try this in 10.3:

http://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/

Otherwise, can you try 10.5?

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,738 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Amreen

I think Erich reply is correct. Is it solve your issue? If yes, please mark his reply as correct answer. Thanks.

Best Regards

Paul

0 项奖励
回复
1,739 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

MCU10.3 is rather old, the most current release is 10.5.

I checked things in MCU 10.5, and I have the VFM4 package available.

You might try this in 10.3:

http://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/

Otherwise, can you try 10.5?

Erich

0 项奖励
回复