KL25Z Custom PCB with Mbed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL25Z Custom PCB with Mbed

1,540件の閲覧回数
luishowell
Contributor I

I'm trying to use a custom board based on the FRDM KL25Z with Mbed, using the 32 pin QFN variant of the same MCU with an 8Mhz oscillator.

I am using the FRDM KL25Z emulating a Segger J-Link to program the external MCU but have had great difficulty in getting the chip to even toggle a pin when using Mbed. When reading back the memory contents it matches the binary file so programming is successful.

To make sure it is not a hardware issue I programming the external chip using the NXP MCUXpresso IDE and KL25Z SDK, with this configuration it worked first time and the pin successfully toggled.

I have spent hours searching online and comparing the mbed and NXP SDK source code and have been unable to find a solution. Why does the NXP SDK work but not mbed? As most of the code for the project has already been written on Mbed using the KL25Z development board it would difficult to switch over.

ラベル(2)
0 件の賞賛
返信
1 返信

1,390件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Luis,

I'm a bit confuse about your board and tools. Do you mean you are using ARM mbed IDE to develop your project? If yes, I'm afraid you have to put this question to ARM mbed community. We have no ideal about this tool.

Regards,

Jing

0 件の賞賛
返信