KL25 and Processor Expert and DAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL25 and Processor Expert and DAC

Jump to solution
2,753 Views
adriangeiger
Contributor II

Hi All

I'm trying to get the CodeWarrior Processor Expert to provide me with a DAC component. Although that's no problem with the ADC, it seems there is an error in Processor Expert concering the KL25 (freedom board so far).

When I activate the filter "show only components available for processor in focused project" the DAC component is not displayed. When I deactivate the filter, the component appears, but when I add it, there's a message in the component inspector saying "target processor does not contain peripheral of this type"; which is certainly not true.

An update search of CodeWarrior has not led to any results; my current version is 10.3.

However, I have seen there is an Init Routine Init_DAC, but have not tested it so far.

Can someone help me out here?

Cheers

Adrian

1 Solution
1,901 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
2 Replies
1,902 Views
BlackNight
NXP Employee
NXP Employee

Hi Adrian,

this example might help:

DAC Example with the Freedom Board | MCU on Eclipse

0 Kudos
Reply
1,901 Views
steve_fae
Senior Contributor I

Thanks Erich.  Your CDC usb project works like a champ as well.