KL25 Bootloader over USB CDC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KL25 Bootloader over USB CDC

跳至解决方案
2,199 次查看
penguintec
Contributor I

Hi,

I am using the KL25.. (on a freedom board).

I am implementing a firmware bootloader over USB com(CDC).

I require a example project for the KL25... only.

and an easy to read application note.

I have read the other application notes (AN2295) and (AN2295) (AN4379) (AN4370)

These discuss too many architectures and have too many exceptions for too may scenarios.

I am not going to use older  freescale parts, I intend to use only KL25.... in my product.

The above application notes are unacceptable.

If a KL25.. application note and USB DFU bootloader example do not exist then I am happy to develop and share my own.

I require

1. PE (processor expert) based flash write example.

2. Information on the KL25 memory architecture

(in a document separate from other processors and architectures)

Thanks !

0 项奖励
回复
1 解答
1,516 次查看
apanecatl
Senior Contributor II

I'm afraid the app notes you already mentioned are the only ones we have released for USB bootloaders. You are welcome to develop your own bootloader, the microcontroller's memory architecture can be found in the device's reference manual, as for the flash write example using Processor Expert, I'm afraid since PE is a rapid configuration tool, you will not find any example of flash writing using PE, however we do have code examples of flash writing in baremetal code. Attached to my response you can find the Kinetis flash driver check it out and let me know if it is of any use.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,517 次查看
apanecatl
Senior Contributor II

I'm afraid the app notes you already mentioned are the only ones we have released for USB bootloaders. You are welcome to develop your own bootloader, the microcontroller's memory architecture can be found in the device's reference manual, as for the flash write example using Processor Expert, I'm afraid since PE is a rapid configuration tool, you will not find any example of flash writing using PE, however we do have code examples of flash writing in baremetal code. Attached to my response you can find the Kinetis flash driver check it out and let me know if it is of any use.

0 项奖励
回复