Thank you Jingjing,
I understand.
> I think the description
>16bit accuracy specifications in table 25 and 26 is tested based on differential pins ADCx_DP0, ADCx_DM0.
>This is the test condition, not a misstype.
But the manual makes little confuse.
If it is talking about test condition. It should "ADC0_DP0, ADC0_DM0", There is no ADC1,2,3_DP0/DM0 on KL25Z.
Also there is ENOB in Table 26
In same page "All other ADC channels meet the 13-bit differential/12-bit single-ended accuracy specifications."
can read
"ADC0_DP1, ADC0_DM1, DP2,DP3, SE8,SEx ADC channels meet the 13-bit differential/12-bit single-ended accuracy specifications."
=> For better effective number, only appear on using ADC0_DP0/DM0 pair, no other includes DP1/DM1,2,3.
Some of guy I working with, were understood like this.
But all pin pair for differential mode had same performance / same ENOB spec.
Thank you for your answer.
Yasu-I