KL24Z32VFT4 programming issue via FRDM-KL25Z OpenSDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL24Z32VFT4 programming issue via FRDM-KL25Z OpenSDA

1,697 Views
hb0038
Contributor II

Hi, 
I tried to program my custom board which has KL24Z32VFT4 processor using FRDM-KL25Z as debugger.

I used MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA as an OpenSDA firmware. But it did not program. But then I tried to debug another FRDM-KL25Z board using another FRDM-KL25Z board. I connected J6 connectors on the both FRDM boards and I was able to program. So that's mean Can't I use MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA firmware to program KL24Z32VFT4? Is it only support for KL25Z?

Thanks
Harsha

Tags (3)
0 Kudos
Reply
1 Reply

1,558 Views
BlackNight
NXP Employee
NXP Employee

No, you only can program the same microcontroller that way (see Programming MKL24Z32VFT4   and especially Using the Freedom Board as SWD Programmer | MCU on Eclipse .

Keep in mind that MSD programming is more of a 'demo' feature, as programming speed will degrade over time.

I hope this helps,

Erich

0 Kudos
Reply