KL17 example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL17 example

3,852件の閲覧回数
marmotte
Contributor I

Hi,

I'm a brand new user of Freescale MCU, and particularly the KL17 family.

I am designing a long battery life device using UART, I2C, IIS, SPI, RTC peripherals, and it would be helpfull to find KL17 example projects, which could help me to start working with Kinetis L series MCU.

I have already installed the last codewarrior and processor expert version, but I can't find a sample project using a KL17. This is the same issue when I want to build a new processor expert project, I only see KL14/15/16Z MCUs, but no KL17.

Thanks in advance for your valuable support.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,056件の閲覧回数
marmotte
Contributor I

Hi,

Thanks for your answers, I'll read those documents, and come back to click on the "Correct Answer" button

0 件の賞賛
返信

3,056件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

KL17 is using most same modules with KL26,  I would recommend to refer KL26 product sample code as a start point.

KL26 sample code based on FRDM-KL26Z could be downloaded from below link:

http://cache.freescale.com/files/32bit/software/FRDM-KL26Z_SC.exe

Wish it helps.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,056件の閲覧回数
mjbcswitzerland
Specialist V

Seb


I never used this with KL17 but if it basically a stripped down version of the KL26 you can also look at

http://www.utasker.com/kinetis/FRDM-KL26Z.html

This includes every thing that you need (apart for the IIS) and will work out-of-the-box with

CW, KDS, IAR, Keil, Rowley Crossworks, Atollic, CooCox, Green Hills, Standalone GCC or VisualStudio

Regards

Mark

Kinetis: µTasker Kinetis support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信

3,056件の閲覧回数
BlackNight
NXP Employee
NXP Employee

From Q1 2014 on, all new devices (and KL17 is a new one) are only supported in Kinetis Design Studio.

So you need to install Kinetis Design Studio with the Kinetis SDK for the KL17.

Erich

0 件の賞賛
返信