KL17 System Register File reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL17 System Register File reset

1,416件の閲覧回数
laurenthenault
Contributor III

Hello,

I'm using the system register file to carry some information after a VLLS1 reset. My data is usually kept but will randomly revert back to all 0.

Is there any reason that could force the register to reset except a power-on reset? 

Thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

1,210件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

The system register file is only reset during a power-on reset. Please verify that your power supply is stable.

You may refer to the following link for VLLS and system register file:

https://community.nxp.com/docs/DOC-332687

0 件の賞賛
返信