KL17 System Register File reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL17 System Register File reset

1,479 Views
laurenthenault
Contributor III

Hello,

I'm using the system register file to carry some information after a VLLS1 reset. My data is usually kept but will randomly revert back to all 0.

Is there any reason that could force the register to reset except a power-on reset? 

Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

1,273 Views
IvanRuiz
NXP Employee
NXP Employee

The system register file is only reset during a power-on reset. Please verify that your power supply is stable.

You may refer to the following link for VLLS and system register file:

https://community.nxp.com/docs/DOC-332687

0 Kudos
Reply