KL16 debugging problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL16 debugging problem

1,231件の閲覧回数
kayathrim
Fresh Out Contributor

Hi all,

We are using KL16 QFN package IC in our board. We are not able to debug continuously. When we are unable to debug, The following error is shown up.

pastedImage_0.png

The status of reset pin is as follows:

1. When debugger is connected
pastedImage_5.png

2. When debugger is not connected


pastedImage_6.png

Please suggest a possible solution for the above problem

Regards,

Kayathri

ラベル(1)
0 件の賞賛
返信
1 返信

1,070件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Kayathri,

Before answer your questions, I'd like to confirm with you about whether the MCU could be downloaded before or not,

I was wondering if you can share the SCH of the debug interface and seek out the issue by yourself through the link as below.

http://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信