KL16 Security Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,471件の閲覧回数
ScottKerstein
Contributor III

Hello,

User code on KL16 runs fine; however, when security fsec is enabled, the micro reset every 1msec.  What could the problem be?

Thanks, in advance,

Scott

ラベル(1)
0 件の賞賛
返信
1 解決策
3,255件の閲覧回数
tommyp
Contributor III

Hi All, I found the problem.  During development, the CodeWarrior flashes via ELF file.  When I attempted flashing Hex from P&E Max, the hex file failed.  I did not output all required sections, resulting in a bad image and the behavior I experienced.

Thanks!

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,256件の閲覧回数
tommyp
Contributor III

Hi All, I found the problem.  During development, the CodeWarrior flashes via ELF file.  When I attempted flashing Hex from P&E Max, the hex file failed.  I did not output all required sections, resulting in a bad image and the behavior I experienced.

Thanks!

0 件の賞賛
返信
3,255件の閲覧回数
tommyp
Contributor III

A little more info.  When secured, the reset line only goes to 2volts.  Unsecured it goes to 3.3v.

0 件の賞賛
返信
3,255件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Tom,

Could you provide more detailed info about your application software?

Which KL16 modules you are using with your application?

And do you have any Flash operation within your application?


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,255件の閲覧回数
tommyp
Contributor III

I flashed a version of the code which stops at POR reset entry and does minimal init to remove any application specific issues.   I'm suspecting that the P&E debugger I'm using is not flashing properly, but since the part is secured, I have no way to confirm beyond the fact the test code is not running.  I'm using a custom trim which the P&E flashes as part of the download process (or should be).   I'm stumped.

0 件の賞賛
返信
3,255件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

I would recommend customer to unlock the KL16 chip with Segger J-Link tool.

More detailed info, please check below link:

https://community.nxp.com/thread/439921?commentID=857127#comment-857127 


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信