KL16 SPI Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KL16 SPI Issue

1,403 次查看
rensuiyi
Contributor I

my code :

I just want to use spi without interrupt and dma.I can not recieve the data and stucked.

Is the spi configured ok?

 gpio_pin_config_t pin_cfg;
    spi_master_config_t spi_config;
    uint32_t sourceclock;
    //config the spi
    
    SPI_MasterGetDefaultConfig(&spi_config);
    sourceclock = CLOCK_GetBusClkFreq();
    spi_config.outputMode = kSPI_SlaveSelectAsGpio;
    SPI_MasterInit(SPI1,&spi_config,sourceclock);
    SPI_EnableFIFO(SPI1,false);

    //config the cs pin
    pin_cfg.pinDirection = kGPIO_DigitalOutput;
    pin_cfg.outputLogic = 1;
    GPIO_PinInit(GPIOD,4U,&pin_cfg);
    
    
    while(1){
            SPI_WriteData(SPI1, 0x01);
            while (0==(kSPI_RxBufferFullFlag&SPI_GetStatusFlags(SPI1)));  //stop here ,never continue!!
    }

0 项奖励
回复
1 回复

1,320 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi ren suiyi,

    About the problem that you can't receive the SPI data,  it may also relates to the slave, did you check the SPI wave from the slave?

   Is the slave send back the SPI data?

   About the SPI code without interrupt and dma, I have the spi driver for your reference, please check it in the attachment, it have the SPI initialization code, and the send receive code.

   Please try my code on your side, whether it works on your side.

   After testing, please let me know your test result, the attached code can work on my KL26 board.

Wish it helps you!

Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复