KL16 Change in Captouch count with change in Temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL16 Change in Captouch count with change in Temperature

1,814 Views
amitmehta
Contributor III

i have added external overlay for captive input, TSI module is configured in auto noise mode. Controller works properly in normal condition but when there is change in temperature value of count decrease with decrease in temperature and increase with increase in temperature. Counter value difference is going beyond 8000 w.r.t. Calibration value.

Is there any way to get touch input while avoiding any false touch input. So that our application can work properly.

Below is configuration done for TSI module :-

TSI Module Setup Parameters

Parameter

Value

Scanning Time Per Channel

20ms

Delta Value

2000

Pre-scalar

16

Reference Charge

32uA

NSCN

18

Auto Noise Mode Setup Parameters

Mode

Automatic Noise Mode

Filter Bits

3 filter bits

Series Resistance

32 kΩ

Labels (1)
0 Kudos
Reply
4 Replies

1,593 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Are you using the TSS library or only the TSI module?

In the library there is an autocalibration function, you can call this function periodically in order to avoid false touch 

Regards

Vicente 

0 Kudos
Reply

1,593 Views
amitmehta
Contributor III

Hi Vicente,

I am using TSI library  API which is available are available in SDK

SDK Version: KSDK 2.2.0 (2017-03-21) for 

Device: MKL16Z64xxx4

OS: Windows, Toolchain: IAR Embedded Workbench for ARM

0 Kudos
Reply

1,593 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

I do not know if you can add Freemaster  in order to see the baseline value and check if this is increasing due the temperature if this is the case you can reset the baseline making a calibration to set a new value for the baseline

Hopes this will help you

0 Kudos
Reply

1,593 Views
amitmehta
Contributor III

Hi,

I am using KL16 in custom made board so i don't think it is possible to add freemaster. Resetting base line ? i don't get it do you mean perform software reset or update calibration value ? If so on what basis should i update ?

0 Kudos
Reply