KL15 UART Stop Bit Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL15 UART Stop Bit Issue

1,283 Views
ylee
Contributor II

I am trying to read UART signal with 38400 Baud, 9 bit data, 1 stop bit and noticed that characters are missed every few characters. After setting a bit output to generate a short pulse  for RX interrupt, I did confirm that the interrupt signal is not generated for every few characters, especially those following 0x00 character.

How can I resolve this?

Yonggon

Labels (1)
0 Kudos
Reply
1 Reply

1,170 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Yonggon,

There without UART stop bit errata info of KL15 product.

I would recommend customer to refer Kinetis L series product UART module validation code for a reference.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply