KL15 ADC VREF Current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL15 ADC VREF Current

1,490 Views
RussellPead
Contributor II

I want to verify the TI REF3033 does not exceed the current or voltage tolerance specs.

1) For the KL15, what is the ADC VREF current min/max and voltage tolerance?

2) Are there any recommend external voltage references to use for the ADC?

Tags (2)
0 Kudos
Reply
1 Reply

1,179 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

HI,

1> KL15 ADC VREFH voltage could up to 3.6V, same with VDDA voltage level. VREFL is same with VSSA. There is no ADC VREF pins current data.

2> In general, we recommend to use VREFH = VDDA, VREFL = VSSA.

Customer could check below link about how to design KL15 ADC module hardware and software to get more accuracy performance:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4373.pdf


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply