KL05Z GUI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL05Z GUI

1,346件の閲覧回数
pedro_cardona
Contributor I

Hello,

I am evaluating a KL05Z dev board. I heard there is a GUI that allows you to manipulate the capacitive touch sensor, LED, and accelerometer.

Does anybody know how I can get a copy of this?

Thanks,

Pedro Cardona

ラベル(2)
0 件の賞賛
返信
1 返信

1,210件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Pedro:

I wonder if you are talking about FreeMaster or Processor Expert, or neither of these. Could you provide more details?

The information and software downloads regarding Freemaster is at the next links:

FREEMASTER: FreeMASTER Run-Time Debugging Tool

In case you refer to processor expert, then for this tool you have 2 options:

1. It is integrated with CodeWarrior IDE, downloadable from the next path:

CW-MCU10: CodeWarrior for MCUs (Eclipse IDE) - ColdFire, 56800/E DSC, Kinetis, Qorivva 56xx, RS08/S0...

2. Also you can get processor expert standalone, without all the development environment:

PE_DRIVER_SUITE: Processor Expert Software, Microcontroller Driver Suite

I hope any of this is what you are looking for.


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信