KL05 UART communication code Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL05 UART communication code Error

Jump to solution
5,319 Views
bhushanmahale
Contributor I

Hello all,

I am new to Kinetis series.. we are using KL05Z FRDM board... I want to use the UART, for that i have tried to generate code using processor expert. But when i have selected the UART as component it is generating the error :

DescriptionResourcePathLocationType
ERROR: Error in the component setting. More details provided by Component Inspector for this componentexternal_intAS1Processor Expert Problem

Please suggest the solution....

1 Solution
5,056 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

When you add a [Serial_LDD] component to KL05 processor expert project, the AS1:Serial_LDD missing the Baud rate setting. You can refer attached [Component Inspector] to add KL05 UART baud rate setting and other UART setting.

Wish it helps.

View solution in original post

0 Kudos
Reply
3 Replies
5,056 Views
Monica
Senior Contributor III

Hello Bhushan,

did that help? Please keep us posted :smileywink:

Best regards,

Monica

0 Kudos
Reply
5,056 Views
bhushanmahale
Contributor I

Hello Monica,

Yes, it worked for me.. Thank You..

5,057 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

When you add a [Serial_LDD] component to KL05 processor expert project, the AS1:Serial_LDD missing the Baud rate setting. You can refer attached [Component Inspector] to add KL05 UART baud rate setting and other UART setting.

Wish it helps.

0 Kudos
Reply