KL05 ,PTA13 ,can't enable pull down

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL05 ,PTA13 ,can't enable pull down

1,356件の閲覧回数
diegocolombo
Contributor IV

Hi

reading the KL05 reference manual i can't find any reason why  PTA13 could not have the pull down enabled.

Moving it by hand in debug mode it can't be set to 0.

Is there any errata about it or is it my fault??

Thanks

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 返信

1,264件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Diego:

This is not an errata. In your KL05 you can only enable Pull Up, but cannot select Pull Down. You can confirm this in the Chip Configuration -> Human Machine Interfaces chapter. See below:

pastedImage_5.png

I hope this clarifies.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信