KL04 Hard Fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL04 Hard Fault

1,640件の閲覧回数
sergigomis
Contributor III

Hi.

I have problems with KL04Z8.

When I try to debug a simple aplication  (One BitIO toogle for example), I can't debug because inmmediatly appears a PS_ISR(Cpu_ivINT_Hard_Fault).

I use a Kinetis Design Studio 1.1.1

I need do special something with CPU configuration ??

Thank's

Sergi

タグ(3)
0 件の賞賛
返信
1 返信

1,404件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

This issue was already discussed, check this thread:

https://community.freescale.com/message/436064#436064

:smileyinfo: Remember posting your questions in a dedicated space, for example Kinetis Design Studio there it will have more visibility.

I hope this information can help you.

Regards,

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信