KL03 write to flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL03 write to flash

4,006 Views
tonyware
Contributor I

Can I write some code in the KL03 to allow it to write a parameter into its flash?  Paramater write tot needed very often, but read frequently

0 Kudos
Reply
6 Replies

3,869 Views
mjbcswitzerland
Specialist V

Hi

Flash parameters are possible with the KL03 as with any other Kinetis part.

See http://www.utasker.com/kinetis/FRDM-KL03Z.html
At the bottom of that page there is a binary that you can try and also a link to a video explaining the operation. All code, including a number of different parameter system options, is available in the uTasker project (allows also simulation of the KL03 and its internal Flash operation).

Regards

Mark

0 Kudos
Reply

3,868 Views
tonyware
Contributor I

Thanks Mark,

Nice little chip, price is about right in volume too.

I'm going to use the KL03 using Forth Inc's SwiftX cross compiler

system and Segger Jlink

Kind regards

Tone

0 Kudos
Reply

3,868 Views
mjbcswitzerland
Specialist V

Tony

I have never used SwiftX cross compiler (and IDE).
What is the advantages compared to the cross compilers and IDEs that are commonly used for Kinetis developments [MCUXpresso, KDS, CW10.x, S32, Atollic, IAR, Keil, Rowley, Green Hills, CooCox etc.] ?

Regards

Mark

0 Kudos
Reply

3,868 Views
tonyware
Contributor I

Dear Mark,

I've been using the Forth Language for nearly 40 years on many, many

projects, big and small. It's never let me down.

  • Fully interactive, like BASIC but hugely more sophisticated NO

BREAKPOINTS NEEDED

  • No linker

  • Easier to read than C code

  • Built-in multi-tasker

  • Built-in Assembler

  • EXTREMELY compact code*

  • Same language and operating system across numerous targets, all

from a single vendor

  • Can extend the cross-compiler as needed. This is quite easy

and can be hugely useful in writing readable code.

  • I once wrote the code for a PLC including its application on a 6801

single chipper, residing in just 4KB. How about that for compact?

https://www.forth.com/

Concerning my future project...

The original version used the ATmega168

Then another variant the ATtiny1634

I was going to use an ATtiny84A on the next one, until I discovered the KL03

I've just done 2 projects on the SilLabs M0+ and fallen in love with 32bits

all of these are in Forth

Kind regards

Tone

0 Kudos
Reply

3,868 Views
mjbcswitzerland
Specialist V

Tony

Thanks for the information. I have heard from others about how good Forth can be but I never used it myself. Also I have never had a customer who used it (or requested it) so I suppose that is why I have also stuck with C. I wonder whether there are any Kinetis peripheral libraries in Forth? (Or TCP/IP stacks and USB libraries suitable for Kinetis parts).

Regards

Mark

0 Kudos
Reply

3,867 Views
tonyware
Contributor I

Dear Mark,

Have a read of this in 'your copious free time' (!!!)

Cheers

Tone

0 Kudos
Reply