KINETIS KE06 EPWM Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KINETIS KE06 EPWM Problem

ソリューションへジャンプ
5,616件の閲覧回数
donghoha
Contributor II

Hello. This is Mr. Dongho Ha

I am trying FTM EPWM using KEXX_DRIVERS_V1.2.1_DEVD example.

My source code is below (using IAR Compliler)

---------------------------------------------------------------------------------------------------------------------------------

#include "common.h"
#include "gpio.h"
#include "ftm.h"
#include "sysinit.h"


#define ACT_LED_Init() GPIOA->PDDR |= GPIO_PTA7_MASK
#define ACT_LED_Toggle() GPIOA->PTOR = GPIO_PTA7_MASK


int main (void)
{
  unsigned char i;

  sysinit();

  ACT_LED_Init();

  printf("\nRunning the FTM EPWM_demo project.\n");
  UART_WaitTxComplete(TERM_PORT);

  // FTM2 is set as edge aligned pwm mode, high true pulse */
  FTM_PWMInit(FTM2, FTM_PWMMODE_EDGEALLIGNED, FTM_PWM_HIGHTRUEPULSE);
  FTM_SetFTMEnhanced(FTM2); //FTMEN enable
  FTM_SetModValue(FTM2, 40000); //update MOD value, 16bit value, 1KHz
  /* set clock source, start counter */
  FTM_ClockSet(FTM2, FTM_CLOCK_SYSTEMCLOCK, FTM_CLOCK_PS_DIV1);
  FTM_SetChannelValue(FTM2, FTM_CHANNEL_CHANNEL1, 0);


  i=0;
  while(1)
  {

    FTM_SetChannelValue(FTM2, FTM_CHANNEL_CHANNEL1, i*400);
    if(i>=100)
    {
       i=0;
    }
    Delay_ms(10);
    i++;
  }
}

--------------------------------------------------------------------------------------------------------------------------------

I used FTM2 channel 1. (GPIO PTC1 FTM2CH1)

This example operate well. (0~100% variation for one second)

Modulation frequency : 1kHz.

But all FTM2 port output 1kHz pulse with fixed duty.

[ PTC0(FTM2CH0),PTC2(FTM2CH2),PTC3(FTM2CH3),PTB4(FTM2CH4),PTB5(FTM2CH5) ]

FTM2CH0~FTM2CH5 output 1Khz pulse regardless of GPIO setting(Input/Output).

I want to operate only PTC1(FTM2CH1) well.

And if FTM Module change , (using FTM0, FTM1) , MCU be halted.

Question1.

I want to operate only PTC1(FTM2CH1) well.

And I want to use other GPIO pins(PTC0, PTC2, PTC3, PTB4, PTB5) for input or output normaly.

Question2.

I want to use FTM0 or FTM1 EPWM well.

I tried 2days.

But I couldn't find any method.

I want help for these problems. 

Thank you.

タグ(4)
1 解決策
5,262件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Did you change SIM->PINSEL0 and PINSEL1? There are some functions you can use in sim.c, like

   SIM_RemapFTM2CH2ToPTD0();  //ptc2
    SIM_RemapFTM2CH0ToPTH0();  //ptc0

Otherwise these pin will always output PWM wave.

Regards,

Jing

元の投稿で解決策を見る

7 返答(返信)
5,262件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Many of the I/O pins are shared with on-chip peripheral functions. The peripheral modules have priority over the I/O, so when a peripheral is enabled, the associated I/O functions are disabled. So if you want to use PTC0, PTC2, PTC3, PTB4, PTB5, you can remap the ALT FTM2 function to other pin. But it seems you can't eliminate them.

Regards,

Jing

0 件の賞賛
返信
5,262件の閲覧回数
donghoha
Contributor II

Hi,

Thank you for answer.

I changed port FTM2 CH1 -> FTM2 CH2 and remapped to PTD0

I tested this program using remap function.

However, the same symptoms are repeated.

PTC0, PTC1, PTC3, PTC4, PTC5 occur pulse.

Thank you.

0 件の賞賛
返信
5,263件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Did you change SIM->PINSEL0 and PINSEL1? There are some functions you can use in sim.c, like

   SIM_RemapFTM2CH2ToPTD0();  //ptc2
    SIM_RemapFTM2CH0ToPTH0();  //ptc0

Otherwise these pin will always output PWM wave.

Regards,

Jing

5,262件の閲覧回数
donghoha
Contributor II

Thank you for answer.

I already tested by remap function.

But same result.

Thank you again.

0 件の賞賛
返信
5,262件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

I try this on FTM_EPWM_demo project. I just add above 2 sentence and the PWM wave on ptc0 and ptc2 stop. Please try it again.

Regards,

Jing

5,262件の閲覧回数
donghoha
Contributor II

I appreciate to you.

I tried this operation by your comment.

I used KINETIS KE06 44pin chip.

It don't have PTF, PTG port.

So I remapped PTC(FTM2) port to PTF(FTM2CH0) and PTG(FTMCH2~FTMCH5).

now PTC0, PT2~PTC5 input/output operate well and FTM2CH1 PWM also.

But I'm disappointed with MCU structure.

Thank you again for you.

0 件の賞賛
返信
5,262件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, I agree with you. It's structure is a bit strange:smileyhappy:

0 件の賞賛
返信