KEAZ64 muddle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEAZ64 muddle

1,977件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

According to the circuit diagram of the FRDM-KEAZ64Q64 the processor is an S9KEAZ64AMLH, which is handled by the user's manual "9KEA64Z64M20SF0RM".
However the processor runs too quickly (FLL is faster than expected) and also the SIM_SCGC is not at the expected location.

If the user's manual "SKEA128Z80M48SF0RM" is however used as guide (would be correct for SKEAZ64AMLH) all works as expected.

Therefore, why is the chip in the circuit diagram and the marking on the chip on the board equal to the 40MHz S9KEAZ64AMLH, but behave as a 48MHz SKEAZ64AMLH ??? What is the source of this confusion?

Regards

Mark

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,707件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Mark,

The S9KEAZ64AMLH and S9KEAZN64AMLH are different chips. For the customer using FRDM-KEAZ64, the chip on that board is S9KEAZ64AMLH. So they need read the KEA128RM.

The part numbers are very similar, sorry for this confusion.

S9KEAZ64AMLH S9KEAZN64AMLH.png

Best Regards,

Robin

0 件の賞賛
返信

1,707件の閲覧回数
mjbcswitzerland
Specialist V

Thanks Robin

It is the N in the name that I was missing (thinking that the S9KEA or SKEA may have been the difference).

Now all makes sense...

Regards

Mark

0 件の賞賛
返信