KEAZ64 Disable NMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEAZ64 Disable NMI

1,448 Views
1915135412
Contributor I

could i disable the NMI interrupt  after system reset ,before into the main function.

like change the flash data or something else.

thanks.

0 Kudos
Reply
1 Reply

1,443 Views
bobpaddock
Senior Contributor III

By definition Non Maskable Interrupts can not be disabled at run time.

Many parts do have a Flash configuration option byte that will either disable NMI completely before executing code or turn it into an alternative function such as enabling the bootloader.

Regardless of that, any NMI pin must not be asserted at reset or allowed to float.
There can be timing races in some parts that cause the NMI to happen before anything else.