KEAZ64 Disable NMI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KEAZ64 Disable NMI

1,449 次查看
1915135412
Contributor I

could i disable the NMI interrupt  after system reset ,before into the main function.

like change the flash data or something else.

thanks.

0 项奖励
回复
1 回复

1,444 次查看
bobpaddock
Senior Contributor III

By definition Non Maskable Interrupts can not be disabled at run time.

Many parts do have a Flash configuration option byte that will either disable NMI completely before executing code or turn it into an alternative function such as enabling the bootloader.

Regardless of that, any NMI pin must not be asserted at reset or allowed to float.
There can be timing races in some parts that cause the NMI to happen before anything else.