KEAZ family ADHWT availability.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KEAZ family ADHWT availability.

跳至解决方案
2,758 次查看
munchosmith
Contributor II

Hi, Dear People,

I need to choose an MCU from the KEAZ###AVL family. I need an ADC conversion hardware trigger, synchronized with the FTM module. It is available, but on a particular MCUs. In the datasheet it's stated, that this is optional. Even more, in the RM (KEA128 Sub-Family Reference Manual, Rev. 2, July 2014), section 24.4.3 Hardware Trigger it's written: " ... This source is not available on all MCUs. See the module introduction for information on the ADHWT source specific to this MCU."

I have problem finding document(s) on the NXP site, that specifies which particular MCUs (part numbers) actually do have ADC hardware trigger implemented.

Please, help me. I'm lost.

Best regards to everyone. Take care.

Mun

0 项奖励
回复
1 解答
2,744 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Muncho,

All KEA128 devices should have this function. Please refer to Table 3-1 in reference manual.

You can refer to this document to get how to trig ADC by PWM.

file:///C:/Users/nxf32199/Downloads/PWM%20signal%20trigger%20ADC%20for%20KEA%20family.pdf

 

Regards,

Jing

在原帖中查看解决方案

2 回复数
2,745 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Muncho,

All KEA128 devices should have this function. Please refer to Table 3-1 in reference manual.

You can refer to this document to get how to trig ADC by PWM.

file:///C:/Users/nxf32199/Downloads/PWM%20signal%20trigger%20ADC%20for%20KEA%20family.pdf

 

Regards,

Jing

2,575 次查看
fanziyu
Contributor IV

The link is broken. Can you fix it?

0 项奖励
回复